Timing profile preferences

Timing profile preferences

Parameter Values Default value Description
ION.SerialConnetion      
ION.TimingProfile

ION.APPLICATION_SETTINGS_ADD_TimingProfile

ION.NewTimingProfile1

Predefined set of ION timing profile preferences.

Note: When you select the default value, all the parameters in the ION.TimingSection become read-only. Create a new ION.TimingProfile to modify the parameters.

ION.Name 1–50 characters ION.NewTimingProfile 1

The ION timing profile name.

Note: Modifying ION.Name will automatically update the ION.TimingProfile name.

ION.HardwareProfile ION.APPLICATION_SETTINGS_HardwareProfile_DirectRS485, ION.APPLICATION_SETTINGS_HardwareProfile_DirectUSB, ION.APPLICATION_SETTINGS_HardwareProfile_OPTICALRS485, ION.APPLICATION_SETTINGS_HardwareProfile_OPTICALUSB, ION.APPLICATION_SETTINGS_HardwareProfile_DirectRS485 Specifies the physical interface used for the communication.
ION.TransmitDelay 0–30000 ms 30 ms Specifies the delay in milliseconds before sending the message.
ION.TransmitInterByte 0–100 ms 0 ms Specifies the delay in millisecond between each byte sent during the message transmission.
ION.ReceiveTimeout 1-60000 ms

3000 ms

Specifies the maximum time in milliseconds to wait to receive a complete message.

ION.ReceiveByteTimeout 1–999 ms 50 ms Specifies the maximum time in milliseconds to wait between received bytes.
ION.RTS

ION.APPLICATION_SETTINGS_RTS_Disabled, ION.APPLICATION_SETTINGS_RTS_FORCEON, ION.APPLICATION_SETTINGS_RTS_FORCEOff, ION.APPLICATION_SETTINGS_RTS_TOGGLE, ION.APPLICATION_SETTINGS_RTS_WaitCTS

ION.APPLICATION_SETTINGS_RTS_Disabled

Specifies the request to send (RTS) signal.
ION.DTR ION.APPLICATION_SETTINGS_DTR_FORCEOFF, ION.APPLICATION_SETTINGS_DTR_Disabled, ION.APPLICATION_SETTINGS_DTR_ModemControl, ION.APPLICATION_SETTINGS_DTR_FORCEON, ION.APPLICATION_SETTINGS_DTR_probecontrol

ION.APPLICATION_SETTINGS_DTR_FORCEOFF

Specifies the data terminal ready (DTR) signal.