Define Dial In Line Properties on a PSTN Outstation

Some PSTN outstations can use a number of PSTN channels to report alarm data to the Geo SCADA Expert server. These channels are referred to as dial in channels as they are used when the outstation ‘dials in’ to the Geo SCADA Expert server. The number of channels varies depending on the outstation type.

Use the fields on the PSTN tab of the associated Outstation Form to define the required Dial In properties. By default, the information in these fields is not set up when you first configure a new outstation.

The following Dial In Lines fields are displayed for outstations on many advanced drivers. For other common PSTN fields, see Define an Outstation’s PSTN Properties, and see Define Dial In Overactive Properties on a PSTN Outstation. For fields that are not described in any of these sections, see the driver-specific documentation.

Prefix Number

Use this field to specify any prefix that needs including at the start of any dial in numbers. Include a number in this field, for example, if the outstation is connected to a local telephone exchange and an additional number (such as 9) is required to dial an external line. The prefix is added to any downloaded dial in Telephone Numbers, and removed from any uploaded numbers.

Location

For each available line, use the Location combo box to define whether the line will be used by the outstation to contact the local Geo SCADA Expert server, or another source:

Local

The channel is used to communicate with the Geo SCADA Expert server that contains the configuration for the outstation (that is, the Geo SCADA Expert server on which you are configuring the PSTN outstation).

Remote

The channel is used to communicate with another source, for example, a handset. The sources that are supported differ, depending on the type of outstation.

If you are defining a line with a Local location, proceed to the Channel field.

If you are defining a line with a Remote location, proceed to the Telephone Number field.

If you are defining a line with a Local location, proceed to the Channel field.

If you are defining a line with a Remote location, proceed to the Telephone Number field.

Channel

Only available for lines that are set to Local. Use the field to specify the PSTN channel that is to be used to communicate with the Geo SCADA Expert server. Use the browse button to display a Reference browse window and choose the required channel. If you are unsure which channels are used, please contact a system administrator, or refer to the system design.

You can only specify a PSTN Channel that is configured as a Dial In Only, or Dial In and Out line (a channel that is configured as Dial Out Only is reserved for the Geo SCADA Expert server to dial out to an outstation). You specify a channel’s Dial In/Out functionality using the PSTN tab on the Channel Form (see Defining PSTN Settings for a Channel).

If your system uses a ‘hunting’ telephone exchange or similar, whereby a pool of PSTN lines share the same telephone number, specify any one of those lines in this field. (The exchange can be local to the site or be provided by a telecoms provider.)

Geo SCADA Expert monitors the channels that are listed in the Channel fields, along with their dial in and dial out properties. If using a ‘hunting exchange’, Geo SCADA Expert also monitors any other channels that share the same telephone number as those listed. Such monitoring is used to determine the state of the outstation. Provided that the outstation is healthy, and at least one channel with dial in capability is available, the outstation will be able to dial in to Geo SCADA Expert when required.

Telephone Number

Only available for lines that are set to Remote. Enter the telephone number of the remote source.

Example:

A particular Geo SCADA Expert system has a number of PSTN lines. The properties of the lines, including their telephone numbers and dial in/out capability, are configured on the relevant PSTN Channel Forms:

(‘PSTN Channel C’ is a dedicated dial out line that the server can use to dial out to the outstations on the system.)

Several of the outstations on the system are able to dial in to Geo SCADA Expert to report alarms. The properties on the PSTN tab of the relevant Outstation Forms are used to specify the PSTN line(s) that the outstations can use to dial in to Geo SCADA Expert. The configuration of one of these outstations is as follows:

The Geo SCADA Expert server monitors the status and dial in/out capability of its PSTN channels, to determine the communications status of each outstation. For the above PSTN outstation, when Geo SCADA Expert is not actually communicating with, or attempting to establish communications with, the outstation via PSTN, the outstation’s status might be one of the following:

Channel Status Outstation State Comments

A, B, and C Healthy

Available

Channels A and B are available for dialing in to Geo SCADA Expert. Channels A and C are available for dialing out.

A Failed, B and C Healthy

Available

Channel B is available for dialing in and channel C for dialing out.

B Failed, A and C Healthy

Available

Channel A is available for dialing in to Geo SCADA Expert. Channels A and C are available for dialing out.

C Failed, A and B Healthy

Available

Channels A and B are available for dialing in to Geo SCADA Expert. Channel A is available for dialing out.

A and B Failed, C Healthy

Available (Outgoing Only)

Channel C is available for dialing out.

A and C Failed, B Healthy

Available (Incoming Only)

Channel B is available for dialing in.

B and C Failed, A Healthy

Available

Channel A is available for dialing in or out.

A, B, and C Failed

All Channels Failed

No PSTN channels are available.