Analog Point Deadband (Asynchronous)

If you are using a server that supports the OPC DA 3.0 protocol and it is configured to read asynchronously, you can also set the Deadband percentage within an item. This allows you to override the Deadband set for the group within which the item resides.

Further Information

Configure the Advanced OPC Server

Asynchronous Polling