Connection State

Associated with: Advanced OPC Servers

The Advanced OPC Server Connection State attribute displays one of the following state values:

  • Disconnected—Geo SCADA Expert is not connected to the OPC DA server. This might be for any of a number of reasons, such as:
    • The server’s configuration is incomplete—for example, the Server ProgID has not been specified (see Checking for Invalid Configuration).
    • The server is not In Service (in which case, the server will typically display an ‘Out of Service’ Quality).
  • Starting—This indicates that Geo SCADA Expert is currently establishing a connection to the OPC DA server. This state is typically fleeting, after which it changes to, either the Healthy or Failed state.
  • Healthy—Geo SCADA Expert has successfully connected to the OPC DA server.
  • Failed—Geo SCADA Expert has not successfully established or maintained a connection to the OPC DA server. To ascertain further information about the reason for this state, use the Display Alarms pick action to display the Server’s Alarms List. or the Event Journal (see Event Lists).
  • Stopping—This indicates that Geo SCADA Expert is currently disconnecting from the OPC DA server. This state is typically fleeting, after which it changes to the Disconnected state.