List of OPC Data Types

Use this section in conjunction with data types that are associated with points in the Advanced OPC Driver.

The following data type is common to all the points that you can configure within the Advanced OPC Driver:

Analog and Digital Point Data Types:

String Point Specific Types

Time Point Specific Types

Further Information

Array Field.