Specify the Model and Type of Radio Unit

The type of diagnostics data that Geo SCADA Expert can retrieve from a Trio radio varies, depending on the radio series and the type of radio unit.

Use the first Model combo box on the Radio tab to specify the radio series, and then use the combo box immediately below it to specify the radio's function in the network (Base, Remote, and so on). The options that are available for the second combo box vary, depending on the radio series chosen in the first combo box.

The options that are chosen for both combo boxes affect:

Further Information

Trio Radio Series Supported by the Advanced Trio Diagnostics Driver.