Display the Alarm Banner

If your User Account enables you to View Alarms, you can view the Alarm Banner if it is not on display.

On a ViewX client or Virtual ViewX client:

  1. Display the Home tab on the ViewX ribbon.
  2. Select Alarm Banner in the Operate command group.

    The Alarm Banner is displayed.