Edit an Existing ViewX Client - System Connection

You can use the Geo SCADA Expert Client applet to change the configuration of an existing ViewX client - system connection. This is useful when you need to alter the way the client - system connection works, for example, you may need to reconfigure the port settings to avoid clashes with other applications.

The settings for a ViewX client - system connection work in exactly the same way as when used during the initial configuration of the client - system connection.

To edit an existing ViewX client - server connection:

  1. Display the Geo SCADA Expert Client Applet.
  2. Select the client - system connection that you want to edit.
  3. Select the Edit button to display the Geo SCADA Expert Client Configuration window (see Display the Client Configuration Window).
  4. Define the System Name and Type for a Client - System Connection.
  5. Enable or Disable Client Licensing.
  6. Define Whether the System is Visible in ViewX.
  7. Define Whether to Connect Client to Fully Synchronized Server Only.
  8. Enable or Disable IPv6 on the Client.
  9. Configure the Client Connection Security Settings.
  10. Define the Workstation Name for the ViewX Client.
  11. Use System Priority for Global Scripts and Homepages.
  12. Define the Node Name for a Client - System Connection.
  13. Define the Node Cost for a Client - System Connection.
  14. Define the Client Compression Settings for a ViewX Client Connection.
  15. Define the Port and Poll Timeouts and Intervals for a ViewX Client Connection.
  16. Change the Range of Ports for the Client’s Incoming Data. (You can ignore this option if all of the clients and servers on your system are running Geo SCADA Expert 2020 or later versions of the software. The Sockets button, Sockets window, and port range for advise links only apply when one or both ends of the connection (server or client) are running a version of Geo SCADA Expert that is earlier than Geo SCADA Expert 2020.)
  17. Associate a ViewX client - System Connection with a Client License.

Alternatively, you can edit the Systems.xml file manually (see Use the Systems.xml File to Set Up a ViewX Client Connection).