Startup Configuration File

The Startup Configuration File is an XML file that you can use to launch Geo SCADA Expert on a Multi-Monitor setup (see Launch a ViewX Client on a Multi-Monitor Setup), and/or have customized Window Container behavior.

You store the Startup Configuration File on the client machine (the machine on which the ViewX client is installed and to which the file relates).

Name the file 'StartupConfiguration.xml' and place it in the following directory:

C:\ProgramData\Schneider Electric\ClearSCADA

(The exception to this is if you use a ViewX command line argument to specify a different name and/or location for the file. You can use such an argument to Define an Alternate Startup Configuration File , whereby you can specify a different name and/or location for each Startup Configuration File that you want to use on a particular client machine.)

If the file is detected when the ViewX client launches, its settings are applied to that client's interface layout, resulting in a Multi-Monitor setup or customized Window Container behavior.

If the XML in the Startup Configuration File is not valid, a diagnostic message will appear when you launch the ViewX client (see Resolve an Invalid Startup Configuration File).

NOTICE

unexpected behavior OF APPLICATION

Startup Configuration files are intended only for use on ViewX clients that are required to launch Geo SCADA Expert on a Multi-Monitor setup, and/or have customized Window Container behavior.
Do not use Startup Configuration files on Virtual ViewX clients, as these clients only support a single monitor setup, and do not support the same customized behavior. Using a Startup Configuration file on such a client could result in unexpected behavior. (Startup Configuration files are not supported, and are ignored, on Original WebX clients.)
Failure to follow these instructions can result in inoperable equipment.

A set of XML Elements is used to define the settings in the Startup Configuration File. You can create and configure the file in any standard XML editing tool.

You can use the Startup Configuration File to: