Source Refresh

Associated with: Simple driver point sources (for example, scanners)

The Source Refresh state is indicated by a flashing blue foreground color, by default.

The color indicates that a Refresh is in progress. A Refresh can be triggered automatically, or manually using the Refresh pick action. If necessary, an ongoing Refresh can be canceled by using the Cancel Refresh pick action.