Types of Point used in Geo SCADA Expert

The type(s) of point that you configure in Geo SCADA Expert varies, depending whether you want Geo SCADA Expert to monitor a device using an input point, or control a device using an output point (for a maintained control) or pulse action (for a pulsed control).

The type of input or output point that you need to configure is determined by:

There are also points used on devices and within Geo SCADA Expert that derive their value from other points, these are called Derived Points. These differ from Internal and Calculation points as they are driver specific and configuration of these points is covered in the driver-specific documentation.

This guide explains how to configure point properties that are common to internal points and to points on many drivers. Many points on drivers have additional properties that are specific to the driver or type of point—these properties are covered in the driver-specific documentation. To configure a point on a driver, we recommend that you refer initially to the driver-specific documentation, as this explains both the driver-specific point properties and refers back to this core guide for those properties that are common to points on many drivers.

This Geo SCADA Expert Guide to Core Point Configuration explains how to configure properties for the following types of point:

Some drivers support other types of point. Configuration of these points is covered in the driver-specific documentation. Many of these points have analog-, counter- or digital-type processing, and therefore many aspects of configuration, explained in this guide, also apply to these point types. The driver-specific documentation indicates when another point type has analog-, counter- or digital-type configuration.