General Point Properties

Use the fields at the top of the DF1 tab to configure the general point properties. The properties are common to points on the DF1 driver—for information, see Configure General Point Properties on the DF1 Tab.