Download File
Associated with: DNP3 master outstations
Security permission required to access this pick action: Retrieve Data
Use the Download File pick action to download a file (for example, an ISaGRAF curve, or a log file) from the Geo SCADA Expert server to a DNP3 outstation.
Select the Download File pick action to display the Download File window. The content of the window varies, depending on the File Transfer Variation supported by the outstation (see Specify Which File Transfer Routines an Outstation Supports).
Where an outstation supports the Revised g70 Variations of File Transfer routines, the Download File window includes these fields:
- Source Filename—Use to specify the name of the file that Geo SCADA Expert is to download to the outstation. The file has to be on the current main Geo SCADA Expert server.
The file has to reside in the folder (or a subfolder within the folder) that is defined using the Server Configuration Tool (see Define the DNP3 Master File Transfer Parameters).
Use the Source Filename field to specify the relative path and filename of the file at the above location.
The folder from which files on the current main server are downloaded to DNP3 outstations is set to:
C:\ProgramData\Schneider Electric\ClearSCADA\Database\DNP3\Master
To download the following file:
C:\ProgramData\Schneider Electric\ClearSCADA\Database\DNP3\Master\My Folder\My File.txt
You set the Source Filename to:
My Folder\My File.txt
- Destination Filename—Use to specify the location (full path) to which Geo SCADA Expert is to download the file at the outstation, and the name that Geo SCADA Expert is to assign to the downloaded file.
The DNP3 outstation may impose filename restrictions on the files that are to be downloaded to it. See the outstation documentation regarding such restrictions.
- Activate—Select this check box to automatically activate the file once it has been downloaded. Files can only be activated automatically on DNP3 outstations that support DNP3 Function Code 31 (Activate Configuration).
Clear the check box (the default) if you do not want the file to be activated after being downloaded.
Where an outstation supports the Legacy g70v1 File Transfer variation, the Download File window includes a single Filename field. Use the field to enter the name of the file that you want to download to the outstation and then select the OK button for Geo SCADA Expert to perform the download.
The location of the file on the server is specified as part of the Geo SCADA Expert
The DNP3 outstation may impose filename restrictions on the files that are to be downloaded to it. See the outstation documentation regarding such restrictions.
Example:
The folder from which files on the current main server are downloaded to DNP3 outstations is set to:
C:\ClearSCADADB
An operator selects the Download File pick action on a particular DNP3 outstation and specifies the filename:
myfile.txt
On execution of the pick action, Geo SCADA Expert downloads the file myfile.txt from the server location C:\ClearSCADADB, to the DNP3 outstation.