Minimum Configuration

As a minimum, you need to configure the following for each DNP3 channel:

You also need to put the channel In Service if you want the channel to be functional (online), and you will need to save the configuration.

Applying these minimum requirements will provide a functional DNP3 channel that uses the default configuration settings.