Specify the Outstation from which Geo SCADA Expert is to Retrieve Status Data

Use the Outstation field on the Parent tab to specify the DNP3 outstation that Geo SCADA Expert is to scan for status data:

Use the field’s browse button to display a Reference browse window and select the required outstation entry from the window.