Status Point Configuration

If Geo SCADA Expert is to retrieve internal status information from a DNP3 device, consider whether to configure DNP3 Status Points in the Geo SCADA Expert database (see Configuring DNP3 Status Points), or individual DNP3 points (see Points Used on DNP3 Outstations).

If you use the former, use each DNP3 Status Points Form to: