Add and Configure the Entries in an IP Route Table

To add entries to a IP Route Table, you need to Display the Table. If the table has insufficient rows, you will need to Specify the Table Size.

You need to add a route entry for each non-local IP address to which a SCADAPack E outstation is to transfer data. There is no need to include entries for IP addresses that are on the same local subnet as the outstation, as data packets will be automatically forwarded to those addresses.

For greatest efficiency, order the entries in a IP Route Table so that routes that are used the most often appear at the top of the table, in priority order (Host, Network, Gateway, and then Default-Gateway). This allows the outstation’s TCP/IP stack to quickly locate the routes that it is to use to transfer most incoming IP data packets.

The entries that you specify in an IP Route Table are persistent (that is, they are retained when the outstation restarts). Any routes that are added using the diagnostic ROUTE command or ISaGRAF function blocks are non-persistent (that is, they will be discarded when the outstation restarts). See the outstation documentation for details on the ROUTE command and ISaGRAF function blocks.

Downloading an IP Route Table to a SCADAPack E outstation will cause a Cold Reset and therefore the loss of any dynamic entries in a table.

Geo SCADA Expert automatically allocates a unique Index number to each entry in an IP Route table. For each entry in the table, you need to specify:

For an example that illustrates how the different route types (Host, Network, Gateway, and Default-Gateway) might be configured, see Types of IP Route.

Use the IP Route Table field on the DNP3 SCADAPack E Outstation Form’s SCADAPack TCP/IP tab to associate the table with a particular outstation (see Specify IP Route and BOOTP Tables).