Configure the Modem Parameters

Use the fields within the Modem Parameters section on the SCADAPack tab to specify the modem properties if the SCADAPack E outstation is to communicate with any device—not just Geo SCADA Expert—using a dial-up modem. Specify each value in the OPC Time Format.