Device Monitor Version

Associated with: DNP3 SCADAPack Status Information items that are configured to retrieve System Overview, or SCADAPack ES Remote I/O information.

This status attribute indicates the version of the Boot Monitor firmware that is running in the outstation or remote I/O module.

Example:

215