Enable Point

Associated with: DNP3 SCADAPack E Trend items

Security permission required to access this pick action: Disable Points

Use the Enable Point pick action to place a Trend item In Service. Triggering the action changes the Trend item’s configuration so that its In Service property is enabled.

If you are using the Enable Point pick action to enable a Trend item that is disabled at the outstation as well as in Geo SCADA Expert, you then need to download the Trend item’s configuration to the outstation, using the Download Configuration pick action.

Providing that the devices on which the Trend item is dependant (such as its parent point and SCADAPack E outstation) are also In Service and have valid configuration, the Trend item will become active.

Also see Disable Point, and see Enable All Trends.

If using this pick action with the Automation Interface, you need to specify the method name Enable.