Enable or Disable TCP/IP Functionality

Use the Enabled check box at the top of the SCADAPack TCP/IP tab to specify whether TCP/IP functionality is enabled for the SCADAPack E outstation.

Select the Enabled check box for the other fields on the tab to become available.

Ensure that the check box is clear if the outstation does not require TCP/IP support.