File Restrictions

The files that you download to a SCADAPack E outstation have to comply with the following conventions. Where a file name needs adjusting to conform to these requirements, you can do this by renaming the file (see Specify the Properties of a File in a SCADAPack E Outstation’s Configuration), rather than renaming the original copy of the file.

If a file does not comply with these limitations or displays any invalid characters, the OK button on the Properties window will appear ‘grayed out’ and unavailable for use.