Frames Received

Associated with: DNP3 SCADAPack Status Information items that are configured to retrieve Port Status information.

This status attribute indicates the number of DNP3 frames that have been received using this port.

Also see Master Frames Received, and see Received CRC Errors.