Off Scan

Associated with: DNP3 SCADAPack E outstations and DNP3 SCADAPack Remote E outstations; DNP3 SCADAPack points and pulse actions

Security permission required to access this pick action: Off/On Scan

Depending on the system configuration, use the Off Scan pick action to place individual points, or outstations and their dependants (such as points and pulse actions) ‘Off Scan’.

The ability to place points and outstations Off Scan is disabled on most systems by default. Its permission is typically denied on a per server basis.

WARNING

UNEXPECTED BEHAVIOR OF APPLICATION

Use the Off Scan pick action on an outstation with care—always check an outstation’s current activity before deciding whether to use this action.

To check whether an outstation is currently processing a request, look at its entry in the Outstations List’s Current Request column. You can also check an outstation’s current activity via, for example, the Events List or the outstation’s Status display.

Failure to follow these instructions can result in death, serious injury, or equipment damage.

When an item is Off Scan:

An Off Scan item differs from an item that is not In Service. An item that is not In Service is not scanned at all and is effectively ignored by Geo SCADA Expert.

To place an individual point or pulse action Off Scan, select the Off Scan pick action from that item’s context sensitive menu.

To place an outstation Off Scan, select the outstation’s Off Scan pick action to display the Off Scan window.

Select the window’s Include Points check box if each of the outstation’s dependants, such as points and pulse actions, are also to be placed Off Scan. No events are generated, or data logged, for any points or pulse actions while they are Off Scan.

Ensure the check box is clear if the outstation’s dependants are to remain On Scan. Although the outstation does not report any data to Geo SCADA Expert while it remains Off Scan, the points and pulse actions will remain ‘live’. As such, the outstation may continue to generate events and/or log data for any On Scan items. Such data will be stored locally at the outstation and be retrieved by Geo SCADA Expert when the outstation is placed back On Scan.

With PSTN or ‘On Demand’ outstations and points and pulse actions on such outstations, the Off Scan window may display a Queue check box. Use the check box to indicate whether Geo SCADA Expert is to perform the request immediately, or queue the request if Geo SCADA Expert is not currently in communications with the outstation (see Queue Check Box in the Geo SCADA Expert Guide to Drivers).

The entry that is logged in the Events List when the Off Scan pick action is triggered on an outstation indicates whether the Off Scan request includes the outstation’s points. Additionally, each item’s Scanning Scanning status attribute indicates whether that item is currently On or Off Scan.

Use the On Scan pick action to return an Off Scan item back to its fully functioning ‘On Scan’ state.