Specify Whether Point Mapping is Used

This section applies to points that have a Point Type of Physical Input or Physical Output. (For other Point Types, the Mapping tab is disabled. This is indicated by the text ‘No Mapping’ being displayed on the tab in place of any fields.)

Use the Mapping combo box on the Mapping tab to specify whether mapping is used to specify the source and location of a point. The options vary, depending on the Outstation Type of the DNP3 SCADAPack E outstation with which the point is associated (see Specify the Outstation Type).

Further Information

Configuring I/O Expansion Cards and Modules.

SCADAPack E Data Concentrators and Remote Outstations.