Specify the SCADAPack Outstation with Which the I/O is Associated

Use the Outstation field on the <I/O Type> tab to specify the DNP3 SCADAPack E outstation with which the I/O expansion card or module is associated.

Use the browse button to display a Reference browse window. Select the relevant outstation from the window. The window is filtered to include only those DNP3 SCADAPack E outstations that have an Outstation Type that supports this particular type of I/O card or module (see Configuring I/O Expansion Cards and Modules).