Specify the SCADAPack TCP/IP Properties

Use the fields on the SCADAPack TCP/IP tab of each DNP3 SCADAPack E Outstation Form to manage the TCP/IP functionality of the outstation. For more information, see the topics that are listed in the gray footer section at the bottom of this topic. Select the relevant entry to display the topic that you require.