UpdateRowDetails

Associated with: DNP3 SCADAPack BOOTP, IP Route, DNP Route Tables, and 32-bit Point Modbus Maps

Security permission required to access this method: Configure

Use this method to update a row in a DNP Route, IP Route, BOOTP table, or 32-bit Point Modbus Map that exists in the Geo SCADA Expert database.

This method is the equivalent of updating the row properties within ViewX (see Configuring DNP3 SCADAPack Tables, or see Configuring DNP3 SCADAPack 32-bit Point Modbus Maps, as applicable).

Use the RowCount configuration parameter to specify the table or map size.

The UpdateRowDetails method arguments vary, depending on the type of database item. For further information, see: