Enable Point

Associated with: Points and pulse actions

Security permission required to access this pick action: Disable Points

Use this pick action to place a point In Service. Triggering the action changes the point or pulse action’s configuration so that its In Service property is enabled. Providing that the devices on which the point is dependant are also In Service and have valid configuration, the point will become active. (Depending on the configuration and type of point, dependants might include the point's scanner, outstation, outstation set, and so on.)

The Enable Point pick action is only available for a point:

  • That is not In Service
  • For which your User Account is allocated the Disable Points security permission.

Also see Disable Point.

If using this pick action with the Automation Interface, you need to specify the method name Enable.