Inching

Associated with: Pulse actions that support user-definable control periods

With pulse actions on some drivers, you can use:

Be aware that triggering an Inching or Control action on a point on a PSTN outstation will result in Geo SCADA Expert executing a One Shot call to that outstation.

The Inching pick action is only available on a pulse action on which:

Select the Inching pick action to display the Inching window.

(The Inching functionality differs for pulse actions on some drivers—the driver-specific documentation explains any such differences.)

For pulse actions on most drivers, these fields are displayed:

The Point Action system color indicates when an inching action is currently active. The pulse action’s Control Active status attribute also indicates whether an inching action is currently ongoing.

The pulse action’s Control Alarm status attribute indicates the success, or otherwise, of the latest Inching or Control action.