ABS

The ABS function is a mathematical function. It returns the absolute value of a number.

Function Name

ABS

Description

Provides the absolute value of a number.

Arguments

ABS(INTEGER or REAL)

The ABS function can have one input and this can be either an integer or a real floating value—see Number (Integer or Real).

Returns

Absolute {Same type as input}

The absolute value of the input. The output value is of the same type as the input value (integer or real).

Example:

ABS(-44)

The output is 44.