TANH

The TANH function is a mathematical function that returns the Hyperbolic Tangent of a number. The TANH function returns a real value.

Function Name

TANH

Description

Returns the Hyperbolic Tangent of a number.

Arguments

TANH(INTEGER or REAL)

Where:

  • INTEGER or REAL is a numerical expression that defines the value on which the TANH function is applied.

For more information on integers and real values, see Number (Integer or Real).

Returns

REAL

The Hyperbolic Tangent of a number.

Example:

TANH(2.9)

The output is 0.99