Learn about the properties in the Tag Names section. Learn about the properties that apply to a Direct Connection. Learn about the properties that apply to a Connection Via Adapter. Learn about the properties in the Connection Characteristics section. Learn about the properties in the Store/Forward section. Learn about the Connection Mode.

Configure an AVEVA Historic Data Export Item

To configure a database item that represents a connection to a historian in an AVEVA application, you have to display the AVEVA Historic Data Export Form (see Display a Form) and configure the relevant settings on that Form.

The figure below is interactive. You can select different parts of the figure in order to access further information about your selection.

The properties on the AVEVA Historic Data Export tab of the AVEVA Historic Data Export form.

The AVEVA Historic Data Export Form has several tabs:

Use the fields on the AVEVA Historic Data Export tab to define the connection properties that enable Geo SCADA Expert to communicate with the historian server:

For information about configuring the other properties on the rest of the AVEVA Historic Data Export tab, see the relevant topics in this section. For more information, see the topics that are listed in the gray footer section at the bottom of this topic. Select the relevant entry to display the topic that you require.

Further Information

Specify the points and/or accumulators for which you want to export historic data using the AVEVA Historic Data Export item: see Define the Historic Export Details in the Geo SCADA Expert Guide to Core Point Configuration.