Specify the Operations Performed on Communications Establishment

When the Geo SCADA Expert server has not been in communications with an IEC 60870-5 outstation for some time, it performs an Establishment Phase scan, rather than the usual Primary Phase scan (see Establishment Phase in the Geo SCADA Expert Guide to Advanced Drivers).

Use the fields within the Communications Procedure section of the IEC 60870-5 tab to specify the operations that the IEC 60870-5 driver performs during an Establishment Phase scan: