Specify Whether the Slave Includes Time Tags in its Data Transmissions

The configuration Form for IEC 60870-5 Slave Direct Outstations and IEC 60870-5 Slave Logical Outstations includes an IEC 60807-5 Application Layer Configuration section. Use the section to specify whether the slave outstation (Geo SCADA Expert) reports its summer time setting or includes time stamps with the data that it sends to its SCADA master (Controlling Station).