Configuring Digital Points

The Kingfisher driver supports 1-, 2-, and 3-bit Digital Input Points and Digital Output Points.

Configure the properties of each digital point using the fields on the Kingfisher Digital Input Point Form, or the Kingfisher Digital Output Point Form, as appropriate.

This section covers configuration of properties on the Digital Point tab of both Kingfisher Digital Point Forms, and the properties on the Control tab for Digital Output points.

 

Use the Digital Point tab to:

 

For Kingfisher Digital Output points, there are two additional tabs: a Control Tab and a Control Checks tab.

Use the Control tab to:

You can optionally use the Control Checks tab to configure the Control Checks settings (see Configuring Control Checks Settings in the Geo SCADA Expert Guide to Core Point Configuration).

For information on the fields on other tabs, see Tabs on Point Forms in the Geo SCADA Expert Guide to Advanced Drivers.