Kingfisher Remote Configuration

For each Kingfisher Remote, you need to configure a Remote Kingfisher Outstation to define the unit that monitors data and control plant (see Configuring a Kingfisher Outstation).

Each Kingfisher Remote communicates with a Kingfisher Master. You need to set up one suite of Kingfisher Master Configuration (see Kingfisher Master Configuration) for each Master-to-Outstation network. For an example of a Master/Remote setup, see Kingfisher Master Outstation with Remote Outstations.