Recommended Settings for Scan Durations

The recommended settings for some of the scan durations vary according to the number of outstations that are associated with the selected direct channel. This section provides the recommended settings for typical system setups (that is, channels associated with 1, 10, 20, 50, 100, and 250 outstations). The settings apply to Kingfisher outstations other than PSTN and Remote outstations, whenever the driver is set to poll the outstations on the channel continuously (that is, each individual outstation’s Polling Interval is set to 0 (zero)).

(With Remote outstations, Geo SCADA Expert retrieves the Master outstation’s copy of each Remote outstation’s data when it scans the Master outstation (see Master and Remote Outstations). Scanning of PSTN outstations differs to that of Direct and Shared outstations (see Retrieving Data from PSTN Outstations in the Geo SCADA Expert Guide to Advanced Drivers).

Scan Interval

 

Number of Outstations

1

10

20

50

100

250

System Scan

5S

15S

30S

1M 15S

2M 30S

5M

Acceptable Scan

10S

30S

50S

2M 5S

3M 45S

8M 20S

Quality Factor (No.)

5

5

5

5

5

5

Minimum Secondary Scan

2S

5S

10S

25S

50S

1M 40S

Max Secondary Scan per O/S

2S

2S

4S

4S

4S

4S

Promoted Scan

10S

10S

10S

10S

10S

10S

Maximum Promoted Scan

5S

5S

5S

5S

5S

5S

Maximum Promoted Secondary Scan

2S

2S

2S

2S

2S

2S

Each Direct channel’s Scan Count status attribute indicates how many scans have completed within the System Scan and Acceptable Scan times that are defined for that channel (see Kingfisher Channel Status Attributes).