Specify a Local System ID (Outstation)

Use the Local Transmit System ID fields on the Kingfisher tab to enable and enter a Local Transmit System ID. This ID  is used to synchronize messages from Geo SCADA Expert to the outstation.

For messages sent from Geo SCADA Expert to the remote outstation, the ID (if enabled) replaces:

NOTE:This only defines the System ID that Geo SCADA Expert adds to the messages it sends to the remote outstation. Messages sent from the remote outstation to Geo SCADA Expert must use either the System ID or the Local System ID set in the Outstation Set.