Welcome to the Geo SCADA Expert Guide to Lists

Welcome to the Geo SCADA Expert Guide to Lists. This guide provides reference information about the various aspects of List operation and configuration.

Intended Audience

This guide is intended for:

Document Scope

This guide explains the types of List that are provided with Geo SCADA Expert, and includes information about:

Geo SCADA Expert is capable of displaying a wide range of information in List form, typically:

For more information, see the topics that are listed in the gray footer section at the bottom of this topic. Select the relevant entry to display the topic that you require.

System administrators or high-level engineers that are setting up the system should see the following section:

In addition to the above, be aware that engineers with the relevant permissions can also optionally configure Custom Lists. Like a standard Queries List, a Custom List uses an SQL query to determine the information that is included in the List. Custom Lists are useful if you want to display information that is not available in any of the standard Queries Lists, or if you regularly want to display a List that is filtered and/or sorted differently.

If you need to use Geo SCADA Expert to query a third-party ODBC database such as an SQL Server database, please refer to Querying Third Party ODBC Databases.