Client Identifier
Associated with: MQTT Broker items
Geo SCADA Expert supports multiple connections to a broker, for which the combined Broker Host Address, Port, and Client Identifier settings have to be unique. This status attribute displays the broker's Client Identifier. This comprises the Client Identifier that is configured on the MQTT Broker's configuration Form.
The Client Identifier on an MQTT Broker has been configured as:
NorthRidge
This is the value that is shown for that Broker's Client Identifier status attribute.
Further Information
Client Identifier: see Configure the Broker Connection Properties.