Introduction to the MQTT JSON Schema A Driver

This driver is an extension driver. It provides additional application-specific functionality to the 'parent' driver with which it is associated. To interact successfully with devices using an extension driver, you need to:

  • Install and run both the extension driver and its 'parent' driver (and, if applicable, its 'grandparent' driver)
  • Ensure that the extension driver and its 'parent' driver (and, if applicable, its 'grandparent' driver) are licensed
    (some extension drivers are licensed separately to their 'parent' driver)
  • Configure the required database items and settings on the 'parent 'driver (and, if applicable, the 'grandparent' driver)
  • Configure the required database items and settings on this extension driver.
  • Ensure that the database items (and any database items on which they depend) have valid, saved, configuration and are 'In Service'.

Intended Audience

This guide is primarily intended for engineers who are responsible for configuring MQTT JSON Schema A driver items and features in the Geo SCADA Expert database.

The guide also contains information for maintenance engineers.

Document Scope

This guide explains the configuration, features and database items that are specific to Geo SCADA Expert’s MQTT JSON Schema A driver. The driver enables Geo SCADA Expert to retrieve data using either of two MQTT JSON Schema A message formats.

WARNING

POTENTIAL SECURITY BREACH

We strongly recommend using network-connected Geo SCADA Expert drivers in a private network only (either physical or virtual). We recommend against using such drivers for communications over the public Internet. If the drivers are used over the public Internet, as a minimum those drivers should use valid SSL certificates to initiate secure connections and encrypt the data that is transmitted over the network.
Failure to follow these instructions can result in death, serious injury, or equipment damage. The breach in system security could expose sensitive data and the leave the database vulnerable to unauthorized and potentially malicious use.

The MQTT JSON Schema A driver is an MQTT extension driver. It provides additional functionality to enable Geo SCADA Expert to retrieve data using either of two MQTT JSON Schema A message formats (see Supported Message Formats).

In order to retrieve data using the MQTT JSON Schema A message formats, Geo SCADA Expert needs to run both the MQTT driver and the MQTT JSON Schema A extension driver (see Confirm that the MQTT JSON Schema A Server Component is Installed).

Use this Geo SCADA Expert Guide to the MQTT JSON Schema A Driver alongside the Geo SCADA Expert Guide to the MQTT Driver. As much of the information in the latter guide is assumed knowledge, we recommend that you read the Geo SCADA Expert Guide to the MQTT Driver before reading this driver guide.

Policy of Continuous Development

To maintain Geo SCADA Expert's position as a leading SCADA solution, we operate a policy of continuous development. Each new version of our product supports additional features and functionality to previous releases. To use the new drivers, features, or functionality involving database items, your system has to be running the latest version of Geo SCADA Expert software. Additionally, if you have upgraded from an earlier version of the product, you have to deactivate any Database Emulation that was activated during the upgrade process. You should only deactivate the Database Emulation once you have successfully completed the upgrade process on all of the servers and clients in your system (see Deactivate Database Emulation after a Successful Upgrade).