Actions that are Specific to Sparkplug™ EoN Nodes

In addition to actions that are common to many database items, Sparkplug EoN Nodes support these item-specific actions:

  • Create Points from Birth Metrics

    Use this pick action to trigger Geo SCADA Expert to create the relevant points to represent the metrics that exist in an EoN Node.

    To create a suite of points for the metrics that exist on any devices on the node, select the Create Points from Birth Metrics pick action on the relevant Sparkplug Devices.

  • Disable EoN Node
  • Display Devices
  • Display Points

    Use this pick action to display a list of points that are directly connected to the EoN Node.

    To display a list of the points that are connected to any devices on the node, select the Display Points pick action on the relevant Sparkplug Device. (To do this, access the pick action as you would any other pick actions. Alternatively, select the pick action from the relevant Device on the Sparkplug™ Devices List that you can display using the Display Devices pick action mentioned below.)

  • Enable EoN Node.

Further Information

Pick actions that are common to many database items: see Object Menu Options in the Geo SCADA Expert Guide to ViewX and Virtual ViewX Clients.