Configure a Sparkplug™ EoN Node

A Sparkplug EoN Node represents an Edge of Network (EoN) node on a Sparkplug Broker. The node is an MQTT version 3.1.1 compliant client application that manages an MQTT session. a Sparkplug EoN Node can be the parent of Sparkplug Devices and/or Sparkplug Points.

You configure the properties of each EoN Node using the fields on the Sparkplug EoN Node configuration Form. The Form has several tabs, some of which contain properties that are common to many database items, and others that contain properties that are specific to Sparkplug EoN Nodes.

The topics in this section document the properties that are on the EoN Node tab (see Configure the Properties on the EoN Node Tab).

The properties on the remaining tabs are common to many database items. For information about those tabs, see Tabs that are Common to Many Configuration Forms.