Errors When Create Points Last Ran
Associated with: Sparkplug™ EoN Nodes and Sparkplug Devices
This status attribute indicates whether Geo SCADA Expert detected any issues when the Create Points from Birth Metrics pick action was last executed on the selected Sparkplug EoN Node or Sparkplug Device.
A value of 0 (zero) indicates that the point creation process that was last triggered by the Create Points from Birth Metrics pick action completed successfully.
If a value other than 0 is displayed, look at the entries in the Alarms List and Events List to ascertain the issues that occurred. The entries will be assigned the Sparkplug Configuration Error category (see Alarm and Event Categories that are Specific to the Sparkplug™ Driver).