Last Import Status
Associated with: Sparkplug™ Property Translation Tables
This status attribute indicates whether Geo SCADA Expert detected any issues when the Import Property Translation Table pick action was last executed on the selected Property Translation Table.
The status attribute displays one of these values:
-
Succeeded—The last request to import a Property Translation Table file completed successfully on this database item.
Ensure that the Property Translation Table is associated with the relevant Sparkplug EoN Node or Sparkplug Device before attempting to use the Create Points from Birth Metrics pick action on the Sparkplug EoN Node or Sparkplug Device (see Configure the Properties on the EoN Node Tab, and see Configure the Properties on the Device Tab). The pick action triggers Geo SCADA Expert to create the suite of database points for the Sparkplug EoN Node or Sparkplug Device. Geo SCADA Expert uses the imported Property Translation Table file to determine which point configuration properties it should set on the points as it creates them. For more information, see Create Points from Birth Metrics, and see Use a Property Translation Table to Configure Automatically Created Points.
-
Never Imported—The Import Property Translation Table pick action has never been used to import a Property Translation Table file on this particular database item.
-
Failed—The last attempt to import a Property Translation Table file on this database item did not succeed. Look at the Events List to ascertain the issue(s) that occurred. The entries will be assigned the Sparkplug Configuration Error category (see Alarm and Event Categories that are Specific to the Sparkplug™ Driver).