Source

Associated with: Sparkplug™ EoN Nodes, Devices, and Points

The Source attribute is common to many Status displays. The attribute indicates the location at which the item resides. The information shown varies, depending on the item.

The Source attribute displays the value Undefined if the item’s configuration is incomplete, in so far as the device with which the item is associated has not yet been specified.

With an item for which the Source content is only partially configured, the unpopulated part of that status attribute is typically indicated by two single straight quotation marks next to each other. Additionally, the item's Current Quality will provide further information about the issue.

 

With a Sparkplug EoN Node, information is displayed in this format:

Broker:'<Broker Host Address>:<Port>' Group:'<Group Id>' EoN Node:'<EoN Node Id>'

 

Broker:'123.0.0.1:8883' Group:'A5' EoN Node:'Nd55'

(For a Sparkplug Eon Node that is configured to use EoN Node Id 'Nd55'. The node is in the Sparkplug Group that is configured to use Group Id 'A5'. The Group is associated with the Sparkplug Broker that has the Broker Host Address 123.0.0.1 and listens on Port 8883.)

With a Sparkplug Device, information is displayed in this format:

Broker:'<Broker Host Address>:<Port>' Group:'<Group Id>' EoN Node:'<EoN Node Id>' Device:'<Device Id>'

 

Broker:'123.0.0.1:8883' Group:'A5' EoN Node:'Nd55' Device:'Dv23'

(For a Sparkplug Device that is configured to use Device Id 'Dv23'. For details about the Eon Node to which the device is connected, along with the Group and Broker with which the EoN Node is associated, see the example above.)

With a Sparkplug Point:

  • Information is displayed in this format if the point is on an EoN node:

    Broker:'<Broker Host Address>:<Port>' Group:'<Group Id>' EoN Node:'<EoN Node Id>' <Point Type>: '<Metric Name>'

  • Information is displayed in this format if the point is on a Sparkplug device that is connected to an EoN node:

    Broker:'<Broker Host Address>:<Port>' Group:'<Group Id>' EoN Node:'<EoN Node Id>' Device:'<Device Id>' <Point Type>: '<Metric Name>'

  • If the point is a digital point, the above Sparkplug EoN node or Sparkplug device content is appended with:

    Digital: '<Metric Name>', Bits <Number of Bits>

     

    Broker:'123.0.0.1:8883' Group:'A5' EoN Node:'Nd55' Device:'Dv23' Digital: 'Switch3', Bits 2

    (For a 2-bit Sparkplug Digital Point that is configured to use the Metric Name 'Switch3'. For details about the Sparkplug Device, and Eon Node to which the device is connected, along with the Group and Broker with which the EoN Node is associated, see the example above.)