Creating a Hyperlink to a Webpage
You can create hyperlinks to webpages. This is useful when you need a Mimic to provide access to information that is stored on a company Intranet or on the Internet.
We strongly recommend that you only link to and open external webpages that are from trusted sources to help prevent potential security risks that are associated with accessing external content.
There are several ways to create a hyperlink to a webpage. In this section, we explain how to create a hyperlink to a webpage by:
- Using the Pick Action Wizard to create a hyperlink to a webpage (see Link to a Webpage by using the Pick Action Wizard).
- Dragging the address icon in a web browser onto a Mimic (see Using Drag and Drop to Create a Hyperlink).
For information on how to use animations to configure a hyperlink to a webpage, see Using Animations to Create a Hyperlink.