Displaying Mimic Diagnostics

You can use the Mimic Diagnostic feature to view statistics about the Mimic on display. The statistics are useful for diagnostic purposes, for example, you can determine whether there is a high level of processing required due to an excessive number of segments (this is common with imported DXF files).

To display the Mimic Diagnostics:

  1. Select the Graphics tab on the ViewX ribbon.
  2. Select Diagnostics in the Views command group.

    The Mimic Details window is displayed. It contains information about the quantity of each type of Mimic item and segment on the Mimic.