Displaying the Animations Window

To access the animation properties for an object, you need to display its Animations window. The Animations window contains a list of the animation properties that are available for the selected Mimic object and shows any expressions that are in place.

To display the Animations window:

  1. Display the Mimic object's Properties window by double-clicking on the Mimic object (with the Mimic in Design mode).
  2. Select the General tab.
  3. Select the Animations button.

Alternatively, right-click on the Mimic object and select the Animations option from the context sensitive menu.

For information on the Animations window settings, see Using the Animations Window.